2015-04-16 1:21 AM
Hello everybody,
first i want to say that im new in the big world of microcontroller,only a basic knowledge. But now i HAVE to work with the STM32F429I-Discovery and the newest Keil uVision v5.15 and the newest CMSIS HAL Drivers. For the beginning i want to use a Uart Port to put some Values on my Console. A simple task i thought but it will not work, there is no output in my putty but ''the driver'' returns no error. Can someone have a look on my Code maybe i forgot something (Enable a clock, wrong frequency , wrong pin config etc.) Some parts of the the code i create with STM32CubeMX but these porgrams do not support the ''package selection''- thing in keil so i put the config code in my keil project. OR a different idea: can someone a keil-project where only the U(S)ART1 is enabled in asynchron and Baudrate 115200 . and send a simple ''A'' over the Pin PA9. Code in next post: #hal #uart #usart #stm32f4292015-04-16 1:36 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.