2009-04-08 11:49 AM
STM32 Internal Bootloader
#bootloader-started-by-software2011-05-17 4:09 AM
STM32F103xx has an internal ROM bootloader residing at address 0x1FFFF000 of about 2K. It runs if the user boots in the System mode and STM32 is reset. I found that the bootloader is accessible at the same address (0x1FFFF000) from the regular user FLASH mode.
Are there any restrictions in calling the bootloader from a FLASH application and then would there be a way to jump to the application after the download? This last feature is supported by the bootloader (command 0x21). -- Thanks, Bogdan2011-05-17 4:09 AM
You can start the internal bootloader by software as following:
1) your mcu must be in system mode 2) set MSP/R13 to value from 0x1FFFF000 (normally 0x20000200) 3) Load address from 0x1FFFF004 (normally 0x1FFFF021) 4) Jump to this address The host pc has to do the rest!2011-05-17 4:09 AM
You can call code in the Boot ROM as you can any other. If you want to run the whole thing, don't expect it to return to your application, or have the clocks/interrupt set in the way you had them.
Generally I would recommend reseting into the Boot ROM so it starts without random clocks and interrupts enabled from your application. In application.c // 1FFFF000 -> 20000200 -> SP // 1FFFF004 -> 1FFFF021 -> PC printf(''Entering Boot Loader..\r\n''); *((unsigned long *)0x2000FFF0) = 0xDEADBEEF; // 64KB STM32F103 NVIC_GenerateSystemReset(); In startup.s ; Reset Handler Reset_Handler PROC EXPORT Reset_Handler [WEAK] IMPORT __main LDR R0, =0x2000FFF0 LDR R1, =0xDEADBEEF LDR R2, [R0, #0] STR R0, [R0, #0] ; Invalidate CMP R2, R1 BEQ Reboot_Loader LDR R0, =__main BX R0 ENDP Reboot_Loader PROC EXPORT Reboot_Loader LDR R0, =0x1FFFF000 LDR SP,[R0, #0] LDR R0,[R0, #4] BX R0 ENDP -Clive2011-05-17 4:09 AM
clive1,
do you know how we can do it in IAR EWARM?2011-05-17 4:09 AM
What version? Not too familiar with IAR EWARM, you'll have to look to see how the startup vector works, and how you might change the startup code. If you want to buy me a copy, I'll create a worked example.
You could look forstartup_stm32f10x_ld.s
__iar_program_startOrstm32f10x_vector.c__program_start Or startup.s With GCC I might look in stm32f10x-vector.c, and add some code in Reset_Handler()2014-01-19 6:14 AM
Hi clive1,
How do this on stm32f051. I tried this without succes, the problem error on startup.s: ldr sp,[r0, #0] ''cannot honor width suffix -- `ldr sp,[r0,#0]' '' if changed to r13: ldr r13,[r0, #0] ''cannot honor width suffix -- `ldr sp,[r0,#0]' ''2014-01-19 7:35 AM
Yes, well the Cortex-M0 only supports a subset of the instruction set.
Reboot_Loader PROC
EXPORT Reboot_Loader
LDR R0, =0x1FFFEC00 ; System Memory STM32F0
LDR R1,[R0, #0]
MOV SP,R1
LDR R0,[R0, #4]
BX R0
ENDP
2014-01-19 7:21 PM
Thanks clive1, it's working now,,,
2015-04-13 8:58 AM
Hi Clive1
Sorry to bring up such an old thread but I am implementing this right now and i wonder if you belive that it is necessery to clear the deadbeaf from the controlling device? We are using this to do firmware over the air updates and the plan right now is to have the controlling software look at the specific address and overwrite it with 0 if it still is deadbeaf. Does it seem like a good approach or should a GO command to the reset vectorbe all that is neededBest regrdsMartinWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.