2015-09-09 12:02 AM
Hi.
Using STM32Cube_FW_F4_V1.6.0 demonstration code for STM32F429I-Disco board, in which USBH is configured to operate in full speed mode on HS pins.I am having custom board where USB MSC device is interfaced with FS pins (DM-PA11, DP-PA12, VBUS-PA9 and USB-ID/USB-OC pins are connected but not configured for now). There is a enable pin at PC6 connected to /EN pin of STMPS2161STR.Now, I have modified the demo code in usb_conf.c file as below.&sharpdefine HOST_POWERSW_PORT GPIOC&sharpdefine HOST_POWERSW_VBUS GPIO_PIN_6/* Private variables ---------------------------------------------------------*/HCD_HandleTypeDef hhcd;void HAL_HCD_MspInit(HCD_HandleTypeDef *hhcd){ /* On STM32F429I-DISCO, USB OTG HS Core will operate in Full speed mode */ GPIO_InitTypeDef GPIO_InitStruct; /*EMBEDDED Physical interface*/ __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); GPIO_InitStruct.Pin = (GPIO_PIN_11 | GPIO_PIN_12); GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FAST; GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* Configure VBUS Pin */ GPIO_InitStruct.Pin = GPIO_PIN_9; GPIO_InitStruct.Speed = GPIO_SPEED_FAST; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* Enable USB HS Clocks */ __HAL_RCC_USB_OTG_FS_CLK_ENABLE(); /* Configure Power Switch Vbus Pin */ GPIO_InitStruct.Pin = HOST_POWERSW_VBUS; GPIO_InitStruct.Speed = GPIO_SPEED_FAST; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(HOST_POWERSW_PORT,&GPIO_InitStruct); /* By Default, DISABLE is needed on output of the Power Switch */ HAL_GPIO_WritePin(HOST_POWERSW_PORT, HOST_POWERSW_VBUS, GPIO_PIN_SET); USBH_Delay(200); /* Delay is need for stabilising the Vbus Low */ /* Set USBHS Interrupt to the lowest priority */ HAL_NVIC_SetPriority(OTG_FS_IRQn, 5, 0); /* Enable USBFS Interrupt */ HAL_NVIC_EnableIRQ(OTG_FS_IRQn);}void HAL_HCD_MspDeInit(HCD_HandleTypeDef *hhcd){ /* Disable USB HS Clocks */ __HAL_RCC_USB_OTG_FS_CLK_DISABLE();}USBH_StatusTypeDef USBH_LL_Init(USBH_HandleTypeDef *phost){ /*Set LL Driver parameters */ hhcd.Instance = USB_OTG_FS; hhcd.Init.Host_channels = 7; hhcd.Init.dma_enable = 1; hhcd.Init.low_power_enable = 0; hhcd.Init.phy_itface = HCD_PHY_EMBEDDED; hhcd.Init.Sof_enable = 0; hhcd.Init.speed = HCD_SPEED_FULL; hhcd.Init.use_external_vbus = 1; /* Link The driver to the stack */ hhcd.pData = phost; phost->pData = &hhcd; /*Initialize LL Driver */ if (HAL_HCD_Init(&hhcd) != HAL_OK) { return USBH_FAIL; } USBH_LL_SetTimer (phost, HAL_HCD_GetCurrentFrame(&hhcd)); return USBH_OK;}and in stm32f4xx_it.c file.void OTG_FS_IRQHandler(void){ HAL_HCD_IRQHandler(&hhcd);}Now, the result is:in usb_core.c USBH_Process(), it doesn't pass this condition. It always shows USBH_BUSY. During this process, pulses are observed at DM and DP pins.case HOST_ENUMERATION: /* Check for enumeration status */ if ( USBH_HandleEnum(phost) == USBH_OK) {/* The function shall return USBH_OK when full enumeration is complete */
USBH_UsrLog (''Enumeration done.'');In interrupt part, upon connecting USB Device it shows SOF interrupt.This project is based on FreeRTOS.What could be the possible reasons for this? Kindly help.Thanks,Chandan #enumeration #stm32f29 #usbmscSolved! Go to Solution.
2015-09-09 3:28 AM
upon setting hhcd.Init.dma_enable = 0;
it works. I spend 3-4 days to find out this. But still in doubt, how this caused the problem.2015-09-09 3:28 AM
upon setting hhcd.Init.dma_enable = 0;
it works. I spend 3-4 days to find out this. But still in doubt, how this caused the problem.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.