STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USB Endpoint question

Posted on August 14, 2015 at 09:35Hi! I used CubeMx to generated USB HID Device example code and  update to F4_Discovery Kit.The default endpoint address is 0x01 and 0x81. I could send data from PC to STM32F4 via USB. and STM32F4 also could send dat...

STM32 bootloader form SD card

Posted on August 21, 2015 at 09:04 Hello ! I have a problem with my bootloader form SD card. I think i try everything, now i don't have any ideas. App in sd card have changed memory start address to 0x08002000 and memory size to 0x0003E000. ...

piotr2399 by Associate II
  • 3432 Views
  • 8 replies
  • 0 kudos

stm32 flash problem

Posted on August 21, 2015 at 17:28i am working on stm32f030cc.i implement user boot loader between 0x08000000-0x08003000 and user application onwards.both works fine.i write protect boot loader area.but when power gone and after that when power on d...

karan by Associate III
  • 822 Views
  • 1 replies
  • 0 kudos

STMF429IGT Usb Bootloader AN3990 [SOLVED]

Posted on August 08, 2015 at 23:44 Hello, I'm trying to run this bootloader on a custom board with a 429IG on it. My target application runs fine, but I need to be able to update on site through usb. So far, the bootloader writes the image o...

0690X000006033vQAA.jpg

STM32F407 knowing the bootloader version

Posted on August 20, 2015 at 20:55Hi !I have a question regarding the bootloader versions on my STM32F407xx boards :Is it possible to determin the version of the bootloader a chip contains either from the text printed on the chip or via SWD wires ?M...

ole2399 by Associate
  • 1007 Views
  • 1 replies
  • 0 kudos

FreeRTOS Dynamic Memory Management (STM32F4)

Posted on August 19, 2015 at 18:42Please see attachment .pdf to see the content I excluded for brevity. I have a project with various communication stacks. Messages arrive through one port, and may be processed locally, or routed to another port. Ad...

ssmail by Associate II
  • 3980 Views
  • 2 replies
  • 0 kudos

Ununderstandable HAL enum behaviour

Posted on July 11, 2015 at 07:41 Hello, I have a very simple issue but ununderstandable for me. Hopping someone could explain me what's happening. I have made the code simple in order to point out the issue: #include ''main.h'...

astree by Associate II
  • 1364 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.