2015-08-20 11:55 AM
Hi !
I have a question regarding the bootloader versions on my STM32F407xx boards :Is it possible to determin the version of the bootloader a chip contains either from the text printed on the chip or via SWD wires ?My system can only use the SPI pins for programming so I need to have the v9 bootloader, I presume that the bootloader is in ROM, so it is not upgradeable if I have a chip with the v3 bootloader ?BR,Ole A. Torvmark #bootloader #stm32f407 #version2015-08-20 12:06 PM
You can read the memory on the STM32 using the ST-LINK Utilities, and save it too a file. This includes the ROM, seem to recall there's a specific address to look at, or that it could be gleaned from the binary if not.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.