2015-11-24 8:24 AM
Hi,
I am working on a project where I am communicating with a capacitive touch sensor via I2C. I have successfully achieved read/write over I2C , and now I would like to use the external device's interrupt line to trigger the reads/writes from the discovery board. I have discovered that I can get interrupts to work in a separate project, and I can get I2C working in a separate project. However, when I bring the two together, my I2C works only(external interrupts no longer work). Any ideas as to what might be happening?? I am also open to suggestions in using an third party library or start from a different example project if that's what you recommend.I am using:1)STM32401 Discovery2)STM32Cube_FW_F4_V1.4.0 code base3)I2C example: examples/I2c/I2C_TwoBoards_ComIT4)External Interrupts example: examples/GPIO/GPIO_EXTI #discovery #stm32f4 #i2c #hal #extiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.