2021-01-29 5:04 AM
Hello all,
I Have tried to implement a code to use a USB to read and write the function as a logging process.
My code is running just fine, and it writes and reads just properly. The only problem is that the MX_USB_Host_Process() loop runs only once, whenever during a single run, the write and read, only once, while I need it to run over and over as it is going to be logger!
So, do you guys have any suggestions that how I can run this loop over and over? (I have put the MX_USB_Host_Process() inside a while loop, but the program does not do the "Application Ready" section in my code)
Any help would be appreciated!
Here are my Switch cases
static void USBH_UserProcess (USBH_HandleTypeDef *phost, uint8_t id)
{
/* USER CODE BEGIN CALL_BACK_1 */
switch(id)
{
case HOST_USER_SELECT_CONFIGURATION:
break;
case HOST_USER_DISCONNECTION:
Appli_state = APPLICATION_DISCONNECT;
Unmount_USB();
break;
case HOST_USER_CLASS_ACTIVE:
Appli_state = APPLICATION_READY;
HAL_GPIO_WritePin(led4_GPIO_Port, led4_Pin, GPIO_PIN_SET);
Mount_USB();
Check_USB_Details(); // check space details
Scan_USB ("/"); // Scan for files and directions
Create_File ("/Alireza.txt");
Write_File ("/Alireza.txt", "AAAAAAAAA\n" );
Update_File ("/Alireza.txt", "OMG12345"\n");
break;
case HOST_USER_CONNECTION:
Appli_state = APPLICATION_START;
break;
default:
break;
}
/* USER CODE END CALL_BACK_1 */
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.