2011-09-01 1:37 AM
Hello,
I have a problem with the ethernet controller DP83848 in combiantion with a STM32F107. I designed a PCB with these two components, I copied a part of the schematic of the STM3210C-EVAL board. I am using the RMII mode so I didn't connect the lines needed for MII. I know the software works because I tested it with the EVAL board. I suspect that the ethernet controller works because I can read and write to it. My problem is that I am getting a lot of false carrier sense errors from the ethernetcontroller so I think it has something to do with receiving data over ethernet. Does anybody have any experience with this problem or the ethernetcontroller? Thank You, Marco #metoo #stm32f107-dp83848-carrier-sense #rmii2011-09-01 5:43 AM
Verify the values of the actually placed components. Double check any parts on the eval schematic for fit/no-fit indications, and against the BOM.
2011-09-01 8:27 PM
Check your transformer and RJ45 connector wiring / pinouts, particularly if you're not using the exact same parts as the eval board. I personally find those components to be the easiest to mess up.
2011-09-02 2:04 AM
Thank you for your reply. I used the same parts as in the EVAL board, I only added some ferrite beads to the 3V3 lines. In the schematic of the EVAL they used 50 ohm resistors for the TD+- and RD+- lines but they fitted 51 ohm and I am using also 51 ohm.
I am using the same connector and same values for the resistors.2011-09-02 2:09 AM
Maybe someone can see something wrong with my schematic.
________________ Attachments : Ethernet.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0rb&d=%2Fa%2F0X0000000bec%2FEHMW.Tc570Se6QAirZDkyCZ4wihF4TaSHuqvzuCVrlk&asPdf=false2011-09-08 7:33 AM
I have exactly the same problem, with basically the same schematic. I used the primary source (J0011D21B) jack, and did not include the ferrite beads. The rest of the schematic is identical. If I find the answer, I will let you know.
2012-03-22 3:29 AM
Hello,
Did you, by any change, solve this issue?I'm expiriencing the same problem.Thanks,Martijn2012-03-24 7:28 PM
for RMII mode, i guess we need to use 50MHz. In the Schm attached, i see a comment related to 25Mhz. Hope this is taken care.
2012-03-26 6:14 AM
Hello,
Try to clock the PHY using Ext. oscillator; for RMII mode, user have to provide the 50 MHz clock by soldering a 50 MHz oscillator (ref SM7745HEV-50.0M or equivalent) on the U3 footprint located under CN3 and also removing jumper on JP5. This oscillator is not provided with the board. For more details, please refer to STM3220G-EVAL evaluation board User manual (UM1057).2012-03-27 6:57 PM
Hi Martijn
Can you pls confirm if this solves your problem ? i hope yes.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.