2021-07-05 11:35 PM
2021-07-06 12:06 AM
Hello @JEnde.1 ,
Short answer is yes and multiple open source projects that implement them can be found on the web (stm32-dfu-bootloader) for example. As a rule of thumb, if the internal flash memory can be reprogrammed by the user software or execution is possible from RAM, a bootloader is always possible regardless of its features.
EDIT: What I wrote above doesn't apply to system memory. Please check @Uwe Bonnes 's response.
Best regards,
@SBEN .2
2021-07-06 12:25 AM
Short answer is no. System memory is factory programmed and can not be changes. However you can have your own bootloader in flash.
2021-07-06 12:32 AM
You're right, I missed that she/he was talking about system memory :)
2021-07-06 12:45 AM
Thank You SBEN for the answer. So far clear for me, but my question was if the so called system memory can be used to store a custom bootloader. As far as I understood the manual there is a bootloader which is programmed by ST during production in the system memory. I would like to use this system memory to store my bootloader to safe flash memory for my application.
2021-07-06 12:49 AM
Hello @JEnde.1 ,
Yeah, I missed that you were talking about the system memory (sorry :) ). As @Uwe Bonnes answered above, it is not possible.
Best regards,
@SBEN .2
2021-07-06 12:59 AM
Ok, I understand. Thank you for your fast response!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.