STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VBUS sensing doesn't work because internal pull-up is activated during USB init rather than when connected - STM32F072

Hi all, I just thought I'd add to the list of questions about USB! :grinning_face_with_sweat:I read AN4879 and it says "when the host presence is detected by the device, the device connects its pull up resistor". This is very clear - first detect the...

UART DMA receive via RTOS

hey therethere is a simple question: how can I receive data on my UART in DMA mode using RTOS? recently I ran a project where I just get all the data right when they arrived using UART DMA. but not I what the whole process to be done using RTOS. how ...

Ala by Senior
  • 5737 Views
  • 11 replies
  • 0 kudos

STM32H747i Lwip support

Hi,In the STM32H7Cube code, There is no LwIP example/Application code for STM32H747-eval. Can anyone direct me towards the same?Or let me know the delta between STM32H743 and STM32H747 LWip configuration.The most important code i need is the ethernet...

VishwasM by Associate
  • 1192 Views
  • 2 replies
  • 1 kudos

STM32L1 FreeRTOS tickless idle with RTC wakeup

Posted on October 20, 2016 at 20:04 I'd like to implement vPortSuppressTicksAndSleep() to put the MCU into sleep or stop mode when there is nothing to do in FreeRTOS tasks. It should be woken up by an EXTI interrupt or RTC wakeup. In my implement...

grzegorz by Associate III
  • 6222 Views
  • 10 replies
  • 0 kudos

USBD_CDC Not working at windows 10

Hi everyone !!I am using a virtual com port (VCP) to conect my device to the computer. Everything was running well till i decide to comunicate with a windowns 10 host. I realized two diferent situations :The first was when i started the device with a...

0693W000008wWLYQA2.jpg
FDigi by Associate III
  • 2057 Views
  • 3 replies
  • 1 kudos

Inquiries about spiritDSP

Inquiries regarding spiritDSP.We are implementing mp3 with DAC DMA using SpiritDSP.The time to play depends on the samplerate and bitrate of the mp3 file.The original time is 3 minutes and 10 seconds,The playback time is different as shown below.The ...

sbaek.11 by Associate II
  • 1931 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.