2018-05-06 1:51 PM
I need lock my firmware on the FLASH. But i need access to firmware from my bootloader. Also i need get any more function from own bootloader.
QUESTION:
When i set RDP level == 1 on stm32f103 all ok. FLASH in lock state and all cool.
But, when i try jumping to my application in RAM from own bootloader i get unknown bugs.. data on the RAM is damaged! =(
why?
ps. when RDP level is 0 - then all ok and work fine! Jump is correctly work and sub-programm in RAM work fine
my JUMP (
jump_addr is RAM offset - 0x2000....
:(void Jump_Execute(uint32_t jump_addr = 0x20005800){
// prepare JUMP uint32_t appJumpAddress = *((volatile uint32_t *)(jump_addr + 4)); void (*GoToApp)(void) = NULL; __disable_irq(); // reset ALL and deInit HAL_GPIO_DeInit(GPIOA, GPIO_PIN_All); HAL_GPIO_DeInit(GPIOB, GPIO_PIN_All); HAL_GPIO_DeInit(GPIOC, GPIO_PIN_All); HAL_GPIO_DeInit(GPIOD, GPIO_PIN_All); HAL_RCC_DeInit(); __HAL_RCC_PWR_CLK_DISABLE(); __HAL_RCC_GPIOA_CLK_DISABLE(); __HAL_RCC_GPIOB_CLK_DISABLE(); __HAL_RCC_GPIOC_CLK_DISABLE(); __HAL_RCC_GPIOD_CLK_DISABLE(); RCC->CIR = 0x00000000; HAL_DeInit(); NVIC_DeInit(); NVIC_SCBDeInit();// reset systicktimer
SysTick->CTRL = 0; SysTick->LOAD = 0; SysTick->VAL = 0;GoToApp = (void (*)(void)) appJumpAddress;
__DMB();__set_MSP(*((volatile uint32_t *) jump_addr)); //stack pointer (to RAM) for USER app in this addressSCB->VTOR = jump_addr; __DSB();//** GO MAIN!
GoToApp(); //** does not jump =( while (1){ } }#bootloader #crash-data #stm32f103We’re moving the ST Community to a new platform to give you a better and more reliable community experience.