2018-04-08 7:52 AM
I am using HAL driver for initializing the timer modules. PWM works just fine on TIM3, TIM14 etc. but it is NOT working on TIM15 Channel-1. (I had a similar problem with TIM1 as well but it worked when I initialized TIM3 together with it). I know TIM1 and TIM15 are advanced timers and HAL driver does initialize a couple of extra parameters. I am attaching the code to this question. Thank you in advance!
int main(void)
{ /*
Initialization codes . . . */MX_TIM15_Init();
TIM_OC_InitTypeDef sConfigOC; sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 150; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; HAL_TIM_PWM_ConfigChannel(&htim15, &sConfigOC, TIM_CHANNEL_1); HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_1); }static void MX_TIM15_Init(void){TIM_MasterConfigTypeDef sMasterConfig;
TIM_OC_InitTypeDef sConfigOC; TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig;htim15.Instance = TIM15;
htim15.Init.Prescaler = 0; htim15.Init.CounterMode = TIM_COUNTERMODE_UP; htim15.Init.Period = 255; htim15.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim15.Init.RepetitionCounter = 0; htim15.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_PWM_Init(&htim15) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim15, &sMasterConfig) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET; sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET; if (HAL_TIM_PWM_ConfigChannel(&htim15, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE; sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF; sBreakDeadTimeConfig.DeadTime = 0; sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE; sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH; sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE; if (HAL_TIMEx_ConfigBreakDeadTime(&htim15, &sBreakDeadTimeConfig) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }HAL_TIM_MspPostInit(&htim15);
}
#stm32 #stm32-timer #tim15 #stm32-stm32cube #tim-pwm #stm32f0-hal2018-04-08 8:29 AM
Make sure the correct F0 target is selected (defines) so stm32f070xb.h is included
Check the IS_TIM_BREAK_INSTANCE macro, ie find-in-files
Try explicitly enabling output
/* Enable the main output */
__HAL_TIM_MOE_ENABLE(&htim15);For auto/local variables make sure they are explicitly cleared, or that all fields are initialized
{
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0}; TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};...
2018-04-09 1:42 AM
Turvey.Clive
- Thank you for your support. Initializing the code like thisdid the trick!TIM_OC_InitTypeDef sConfigOC = {0};
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 150;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.