2016-06-23 9:16 PM
Hi,
I'm working on stm32f0 discovery board and using STM32Cube FW v1.5 libraries.As I tested the freertos example ''FreeRTOS_ThreadCreation'' with sending a string in ''LED_Thread1'' and ''LED_Thread2'' functions, then the platform will stuck.It's no problem to send the string in main, so I thinks the GPIO and Uart functionalities should be fine.If I didn't send the string in thread callback functions, the platform was okay too (I can see the LED blinking).I was wondering if it's allowed to use HAL_UART_Transmit in thread callback function. If yes, would you give me some suggestions to fix it.Thanks,Michael #uart #cubemx #freertos #cubeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.