2014-10-03 6:05 AM
Hello forumers... I am evaluating MCUs for use in a device which sits on a CAN Bus network. I need to be able to push firmware upgrades over the CAN bus from a PC.
So far I have found that for my app there is not a suitable MCU available from ST. I just wanted to check on the forum that I am correct in this conclusion. After reading up on the STM32 series I find that the optimal device for me would be the F072, but it seems not to be possible to use the CAN i/f on this device for firmware upgrades. The smallest device I have found which supports CAN bootloading is the F105, but that is way to complex for my application. Best regards /jesper #stm32-can-bootloader2014-10-03 7:51 AM
Beyond initial programming, any part can implement it's own IAP using any interface you choose.
2014-10-03 9:42 AM
Obviously. Anything is possible in software, right?
But that was not my question. My question was if I was correct in understanding that the F105 is the smallest part where the factory bootloader supports CAN.2014-10-03 10:06 AM
You did say ''upgrade'' so IAP is more critical than ISP. It's a lot easier to factory program via USART, and test-points, than CAN.
I haven't done the due intelligence on ISP CAN support across the range, you'd probably want your local ST rep to help you do that.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.