2016-01-19 10:10 AM
I ran my project settings through the CubeMX program to see if there would be any difference in the settings CubeMX makes. I made one observation that seemed worth mentioning.
The systick IRQ priority is set twice:in main.c:void SystemClock_Config(void){.......... /* SysTick_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}in stm32fxxx_hal_msp.c:void HAL_MspInit(void){ /* USER CODE BEGIN MspInit 0 */ /* USER CODE END MspInit 0 */ __SYSCFG_CLK_ENABLE(); /* System interrupt init*/ /* SysTick_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0); /* USER CODE BEGIN MspInit 1 */ /* USER CODE END MspInit 1 */}To me, this seems wrong. In my working project, I have it set in the MSP file and not in main. Has someone experienced this and have any insight on this? #stm32cube #bug #hal #systick2016-02-05 6:57 AM
You are correct:
From the main.c file, the NVIC_setPriority is called 3 times: 1/ once via the HAL_Init that calls HAL_MspInit() that calls HAL_NVIC_SetPriority. 2/ via SystemClock_Config that calls HAL_SYSTICK_Config that calls SysTick_Config (CMSIS-core function hard coding priority value) that calls NVIC_SetPriority 3/ via SystemClock_Config, Last call is HAL_NVIC_SetPriority(SysTick_IRQn, 4, 0); This latter one reflects actual user configuration done in MX user interface.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.