STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeF1 I2C DMA Driver Questions

Posted on January 08, 2016 at 17:15I am attempting to port the ''I2C_TwoBoards_ComDMA'' example project to run on a different target board (ZMDI ZWIR451x Development Board) using Rowley CrossStudio as an IDE.  This target has an STM32F103RC micro.Af...

clark2 by Associate II
  • 1500 Views
  • 3 replies
  • 0 kudos

DfuSe and Windows 7

Posted on January 08, 2016 at 15:11I am trying to get the DfuSe application to work with my STM32 F0 discovery board (running a STM32F051R8T6 micro).  I am using a Windows 7 x64 OS.  Essentially my issue is that the Discovery board is not recognize...

0690X00000605ItQAI.png
cpaye by Associate II
  • 2505 Views
  • 4 replies
  • 0 kudos

Product Level Bootloader

Posted on January 07, 2016 at 20:58Hi, Are there any reference designs for how to implement Boot0 in an end-user product. The boot0 pin is not available external of the product casing. Is there any auto-detect/MOSFET kind of method? Regards, Tom ...

USB OTG Host AND USB HID Device

Posted on January 07, 2016 at 20:11Hi, I am wishing to develop a product that could be auto-detected as a USB OTG Host if for example plugged into an Android device OR would be detected as a USB HID device is plugged into a PC. Ideally in either cas...

VCP Read - Still unclear

Posted on January 05, 2016 at 20:55I am using the STM32F072B-Discovery board and used the CDC_Standalone example to communicate with the PC using a Virtual Serial Port. I am using the VCP driver from the website.I can send data from the microcontrol...

hassan2 by Associate II
  • 2557 Views
  • 4 replies
  • 0 kudos

Nucleo F303RE Problems with Android USB OTG

Posted on January 04, 2016 at 04:01I am trying to plug a Nucleo F303RE into an Android 6.0 phone and connect to the CDC port via an Android application.Bad things happen when I do this.  Apparently Android 6.0 detects the ST/LINK mass storage device...

HAL UART IT stm32f091RB

Posted on December 31, 2014 at 21:13 Hello. for starters, I'm a beginner. So I want to use UART of STM32F091RB and for this I used STM32CUBEMX, and I found much difficulty, so I'll ask my questions. in my program I do not know when I will ...

rafik by Associate II
  • 776 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.