2019-01-14 12:43 AM
STM32L476RCTx
STM32Cube FW_L4 V1.13.0
stm32l4xx_hal_adc.h:
#define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_CH4) /*!< ADC group regular conversion trigger from external IP: TIM4 TRGO. Trigger edge set to rising edge (default setting). */
#define ADC_EXTERNALTRIG_T4_CC4 (LL_ADC_REG_TRIG_EXT_TIM4_CH4) /*!< ADC group regular conversion trigger from external IP: TIM4 channel 4 event (capture compare: input capture or output capture). Trigger edge set to rising edge (default setting). */
must be
#define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_TRGO) /*!< ADC group regular conversion trigger from external IP: TIM4 TRGO. Trigger edge set to rising edge (default setting). */
#define ADC_EXTERNALTRIG_T4_CC4 (LL_ADC_REG_TRIG_EXT_TIM4_CH4) /*!< ADC group regular conversion trigger from external IP: TIM4 channel 4 event (capture compare: input capture or output capture). Trigger edge set to rising edge (default setting). */
2019-01-15 1:42 AM
Hello @dino0410 ,
Thank you for your reported issue.
We confirm this bug and raise it internally for fix.
The definition of ADC_EXTERNALTRIG_T4_TRGO should be updated as followed:
#define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_TRGO).
Kind Regards,
Imen.
2019-04-15 8:29 AM
Hi,
This issue is fixed in the new release STM32CubeL4 V1.14.0.
Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.