cancel
Showing results for 
Search instead for 
Did you mean: 

Hallo Knowing that several interfaces (USART1, USART3, CAN, USB) can interface to the embedded bootloader I wonder if there is any requriments for levels on thise pins when we want to use a specific interface?

Mik
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Yes

By pulling BOOT1 pin to HI during power on reset the device boots from system memory in witch resides the embedded bootloader.

AN2606 contains information for all mcu families how to configure and select the embeded bootloader

Clive1 (HNL)
Senior II

It is sensitive to signals on all the usable interfaces, make sure the one you plan on using is the only one the loader sees activity on when operating in this mode.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.