2024-09-01 11:40 AM
Hello ...
I cloned the github repo:
https://github.com/STMicroelectronics/STM32CubeL4/tree/master
I am trying to compile the PWR_STOP1_RTC project but keep getting a fatal error
../../../../../../../Drivers/STM32L4xx_HAL_Driver/Inc/stm32l4xx_hal_def.h:29:10: fatal error: stm32l4xx.h: No such file or directory
where can I find this file to include within the ....Drivers/STM32L4xx_HAL_Driver/Inc?
Thanks
Solved! Go to Solution.
2024-09-01 1:04 PM
For a succesful clone of this repository. The only way is to use the command
git clone --recursive https://github.com/STMicroelectronics/STM32CubeL4.git
And dont forget the recursive.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-01 12:04 PM
Hello @SWenn.1
This file does exist : https://github.com/STMicroelectronics/cmsis_device_l4/tree/a2530753e86dd326a75467d28feb92e2ba7d0df2/Include.
For the clone operation, have you used this command:
git clone --recursive https://github.com/STMicroelectronics/STM32CubeL4.git
If you didn't added the --recursive or you have downloaded directly the repository as. Zip, that will create a compilation problem.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-01 12:47 PM
I cloned everything but for some reason under the Driver section BSP / STM32L4xx_Nucleo and CMSIS/Device/ST did not come down when I cloned....I had to go up and look into these spaces on github, go to my local area, clone them each separately and then set up the linked files space....
All in all it wasn't very clean as one would hope but I do have things working at this end.
Thanks
2024-09-01 1:04 PM
For a succesful clone of this repository. The only way is to use the command
git clone --recursive https://github.com/STMicroelectronics/STM32CubeL4.git
And dont forget the recursive.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.