2026-05-20 5:50 AM - edited 2026-05-21 7:55 AM
I'm using the latest library provided by the STM32Cube_FW_G0_V1.6.3, specifically STM32Cube_FW_G0_V1.6.3\Drivers\CMSIS\DSP\Lib\ARM\arm_cortexM0l_math.lib
but when using IAR 9.20 I'm having the warning
Warning[Lt009]: Inconsistent wchar_t size
arm_sin_f32.o(arm_cortexM0l_math.lib) and 1 other objects in arm_cortexM0l_math.lib have wchar_t size 16 bits
my_file.o and 54 other objects, some of them in rt6M_tl.a and 5 other libraries have wchar_t size 32 bits How do I avoid the mismatch?
I would like to avoid to link the source code for the cortex M math library and compile it myself.
2026-05-20 2:24 PM
In your main project, how is wchar_t defined? Do you use any text functions (trace, logs...) with wide chars?
See also:
2026-05-21 8:02 AM
I'm using stdlib.h and stddef.h, which define
#ifndef _WCHART
#define _WCHART
typedef _Wchart wchar_t;
#endifBut I'm not directly defining it nor using trace, logs, or any text function.
2026-05-21 11:27 PM
Well then just ignore this warning, build and test your program. If it crashes or behaves weird, see the above link.
2026-05-21 11:50 PM
This usually happens due to a mismatch between the STM32Cube firmware package and the toolchain/precompiled libraries.
Try doing a clean rebuild and make sure your CubeFW version and compiler settings match exactly — in many cases that fixes the wchar_t / math lib inconsistency issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.