2026-03-04 3:09 AM
Dear. All
I'm asking how to use STemWin on stm32h743 mcu.
How to add STemWin on STM32CubeIDE? (Current Use Version. 1.13.0)?
How can I run a project with the development board I bought? (STM32H743I-EVAL)?
In particular, I want to run the STemWin_SampleDemo project.
I`m use IAR EWARM ver 9.xx but in stm32cubeh7-v1-12-1 and
STM32Cube_FW_H7_V1.11.0
\Repository\STM32Cube_FW_H7_V1.11.0\Projects\STM32H743I-EVAL\Demonstrations\STemWin
i find STemWin.ewp project which use OGLastSavedByProductVersion 8.20.2.14834.
It mean`s STemWin.ewp should compile on EWARM 8.20 or late.
Is it possible to use example on later version EWARM ?
Best regards.
Solved! Go to Solution.
2026-03-05 7:51 AM - edited 2026-04-28 10:18 AM
Hello,
1- TouchGFX is something (a ST graphical library), STemwin is something else (SEGGER library).
2- I don't have idea why that was removed but you can download the older version of CubeH7 1.12.0 as shown in this screenshot and use the latest version of IAR.
The library is located under Middlewares\ST\STemWin\Lib
2026-03-04 3:20 AM
Hello,
Normally you can use the latest version of IAR to compile and upload that example to your Eval board. Did you face an issue?
2026-03-04 8:30 AM
Thanks for the answer.
Does ST produce new versions STemWin for stm32h743 mcu ?
Is STM32Cube_FW_H7_V1.11.0 last version for stm32h743 mcu?
2026-03-04 10:32 AM
You can begin from the ST examples for STemWin, then, if you want, update to the latest Segger version.
2026-03-04 11:59 AM
The STemWin library available in the package is the last version we can provide.
The last H7 Cube HAL is V1.13.0
2026-03-05 6:13 AM
Hello all`s.
mƎALLEm good answer.
I `m use STM32CubeMX Version 6.17.0.
And Embedded Software Packages Manager show me next detail about
STM32Cube MCU Package for STM32H7 Series -- installed Version 1.13.0.
Details:
"
STM32CubeH7 Firmware Package V1.13.0 / 04-February-2026 Main Changes
General updates to fix known defects and enhancements implementation.
This new version of STM32CubeH7 package does not contain the graphical middleware stacks TouchGFX and STemWin anymore.
Following related project examples for Evaluation boards and Discovery kits have been removed as well:
Demonstrations
STemWin applications
The ClockAndWeather WiFi application for the STM32H735G-DK board
TouchGFX solution is distributed in a separated X-CUBE-TOUCHGFX package.
STemWin is available from SEGGER."
This info plased in .\STM32Cube_FW_H7_V1.13.0\_htmresc\ReleaseNotes.html
file.
It mean`s This new version of STM32CubeH7 package does not contain the graphical middleware stacks exactly.
Isn`t it?
I start to develop my own project with a graphical LCD on STM32H743I-EVAL Evaluation boards. It`s important have actual version emWin.
2026-03-05 7:51 AM - edited 2026-04-28 10:18 AM
Hello,
1- TouchGFX is something (a ST graphical library), STemwin is something else (SEGGER library).
2- I don't have idea why that was removed but you can download the older version of CubeH7 1.12.0 as shown in this screenshot and use the latest version of IAR.
The library is located under Middlewares\ST\STemWin\Lib
2026-03-05 7:57 AM
According to this 2021 post, STemWin was removed from CubeMX since V5.5 release ...
2026-05-22 12:20 AM
Hello @Andrij Markovsky.
ST discontinued STemWin a few years ago. This means it is no longer free for new projects, and it has not been included in STM32CubeMX for quite some time.
That said, emWin is still an active GUI library, and SEGGER remains a valued ST partner. They continue to invest in supporting selected new STM32 devices.
ST’s investment in GUI software is focused on TouchGFX, which brings better UI performance, ease of use, and technical support benefits for STM32 users. In parallel, ST is also partnering with alternative GUI software providers such as SEGGER.
Best regards,
Johan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.