2018-07-26 9:11 AM
In the file \STM32Cube_FW_F7_V1.12.0\Drivers\STM32F7xx_HAL_Driver\Src\stm32f7xx_hal_pcd.c at line 144 is the instruction: assert_param(IS_PCD_ALL_INSTANCE(hpcd->Instance))
However, I cannot find the macro IS_PCD_ALL_INSTANCE defined anywhere. Note that in STM32Cube_FW_F7_V1.11.0, this macro was defined in \STM32Cube_FW_F7_V1.11.0\Drivers\STM32F7xx_HAL_Driver\Src\stm32f7xx_hal_pcd.h at line 315 and 316.
2018-07-26 12:33 PM
Would appear to be missing
2018-08-15 1:56 AM
Same issue here with v1.12.0:
Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_pcd.c:154: undefined reference to `IS_PCD_ALL_INSTANCE'
2018-08-15 12:36 PM
Same issue here
2018-09-06 10:59 AM
Me too. It was in v1.11.0 and it is missing in 1.12.0
Is there a way to revert a project? How about rolling back Cube to 4.26?
2018-09-06 12:29 PM
Doesn't CubeMX let you remove things? Could swear it did. Back out F7 1.12.0
Anyway got a large mirror of CubeMX releases here, and libraries.
2018-09-10 5:00 AM
Thanks for the confirmations. I couldn't figure out where to submit bug reports, so was hoping ST would see this. If anyone could point me to a better place to submit, I would appreciate it.
As you can see, this bug only matters when assertions are enabled, which I typically do. But I also use quite a bit of my own assertions so I have disabled ST's assertions for now.
2018-09-10 8:14 AM
This is as good a place as any. Will flag it. @STOne-32
2018-09-19 9:20 AM
Hello,
This regression issue is tracked internally and should be fixed in coming versions of STM32CubeF7 package.
Sorry for such inconvenience.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-12-12 8:03 AM
Bug is still there in V1.14.0 !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.