2020-09-03 3:10 AM
Hey. Just found a possible bug here
static void MX_ETH_Init(void)
{
/* USER CODE BEGIN ETH_Init 0 */
/* USER CODE END ETH_Init 0 */
/* USER CODE BEGIN ETH_Init 1 */
/* USER CODE END ETH_Init 1 */
heth.Instance = ETH;
heth.Init.AutoNegotiation = ETH_AUTONEGOTIATION_ENABLE;
heth.Init.PhyAddress = DP83848_PHY_ADDRESS;
heth.Init.MACAddr[0] = 0x00;
heth.Init.MACAddr[1] = 0x80;
heth.Init.MACAddr[2] = 0xE1;
heth.Init.MACAddr[3] = 0x00;
heth.Init.MACAddr[4] = 0x00;
heth.Init.MACAddr[5] = 0x00;
heth.Init.RxMode = ETH_RXINTERRUPT_MODE;
heth.Init.ChecksumMode = ETH_CHECKSUM_BY_HARDWARE;
heth.Init.MediaInterface = ETH_MEDIA_INTERFACE_RMII;
/* USER CODE BEGIN MACADDRESS */
/* USER CODE END MACADDRESS */
if (HAL_ETH_Init(&heth) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ETH_Init 2 */
/* USER CODE END ETH_Init 2 */
}I think it will be better to add something like this
uint8_t MAC[6];
heth.Init.MACAddr = MAC;before any initialization. Am I right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.