2025-05-09 7:51 AM
To test a USB implementation, I have implemented a USB loopback on a Nucleo-144 Development Board (MB1404C). Testing is showing a strange result that I have been unable to isolate:
The code is very basic: it creates a thread for USB data handling. In that thread, ux_device_class_cdc_acm_read is used to block until data is received from USB. When it is received, it is send back out USB using ux_device_class_cdc_acm_write.
This works great if I send up to 6 bytes of data. As soon as I send 7 or more bytes, the transmitted data is junk (though it is repeatable).
Things I have tried and seemingly ruled out:
Any ideas?
2025-05-12 2:48 AM
Hello @Brett21
This post has been escalated to the ST Online Support Team for one-to-one assistance. We'll contact you directly.
Best regards,
Lina
2025-05-12 2:49 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.