2018-06-14 9:20 AM
Hi everyone,
I am currently using USB Full-Speed for an application and I would like to know if there is a way to implement DMA to access USB FS FIFO.
I know that a dedicated DMA exists for USB High Speed but I can not find something similar for Full Speed. Moreover, the documentation and ressources about the FS FIFO remain a bit confusing and could suggest it may be possible to access buffers via DMA but I still didn't manage to do this.
I would need some peace of advice on how I could achieve and implement a such architecture.
Thank you in advance.
#stm32-usb-dma #usb-fsSolved! Go to Solution.
2018-06-14 2:30 PM
I haven't tried, but I see no reason why you shouldn't be able to perform a memory-to-memory DMA using DMA2 (in 'F2/'F4/'F7) with one port pointing to the respective USB_FS FIFO area, just in the same way as you'd copy data from/into USB_FS FIFO using the processor.
JW
2018-06-14 2:30 PM
I haven't tried, but I see no reason why you shouldn't be able to perform a memory-to-memory DMA using DMA2 (in 'F2/'F4/'F7) with one port pointing to the respective USB_FS FIFO area, just in the same way as you'd copy data from/into USB_FS FIFO using the processor.
JW
2018-06-15 8:16 AM
Indeed!
After a few tries it reveals that it is totally possible to access USB_FS FIFO using DMA2. It might though be a bit tricky as it seems important to wait for the transfer to be complete and disable DMA after each transmitted packet!
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.