2017-10-19 2:11 AM
(note this is my first question on ST community If I can do anything to improve the question, please let me know).
Setup
I am using an STM32F103C8T6 (aka Blue Pill).
With the STM32Cube I set CAN_RX to PB8 and CAN_TX9 to PB9 (these are defaults/nonchangeable).The generated CAN settings are:
hcan.Instance = CAN1;
hcan.Init.Prescaler = 16;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SJW = CAN_SJW_1TQ;
hcan.Init.BS1 = CAN_BS1_4TQ;
hcan.Init.BS2 = CAN_BS2_5TQ;
hcan.Init.TTCM = DISABLE;
hcan.Init.ABOM = DISABLE;
hcan.Init.AWUM = DISABLE;
hcan.Init.NART = DISABLE;
hcan.Init.RFLM = DISABLE;
hcan.Init.TXFP = DISABLE;�?�?�?�?�?�?�?�?�?�?�?�?
Program
(removed STM HAL generated comments blocks) int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CAN_Init();
/* USER CODE BEGIN 2 */
hcan.pRxMsg = &_rxMessage;
hcan.pTxMsg = &_txMessage;
_sFilterConfig.FilterActivation = ENABLE;
_sFilterConfig.FilterNumber = 0;
_sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
_sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
_sFilterConfig.FilterIdHigh = 0x0000;
_sFilterConfig.FilterIdLow = 0x0000;
_sFilterConfig.FilterMaskIdHigh = 0x0000;
_sFilterConfig.FilterMaskIdLow = 0x0000;
_sFilterConfig.FilterFIFOAssignment = 0;
_sFilterConfig.BankNumber = 14;
if (HAL_CAN_ConfigFilter(&hcan, &_sFilterConfig) != HAL_OK)
{
Error_Handler();
}
hcan.pTxMsg->StdId = 0x321;
hcan.pTxMsg->ExtId = 0x01;
hcan.pTxMsg->RTR = CAN_RTR_DATA;
hcan.pTxMsg->IDE = CAN_ID_STD;
hcan.pTxMsg->DLC = 2;
hcan.pTxMsg->Data[0] = 0;
while (1)
{
hcan.pTxMsg->Data[0]++;
if (HAL_CAN_Transmit(&hcan, 10) != HAL_OK)
{
Error_Handler();
}
HAL_Delay(1000);
if (HAL_CAN_Receive_IT(&hcan, CAN_FIFO0) != HAL_OK)
{
Error_Handler();
}
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Loopback mode
When I use loopback mode:hcan.Init.Mode = CAN_MODE_LOOPBACK
instead of Normal mode, I can transmit and receive messages (and the hcan shows the correct data in the received message).
Problem
However, in Normal mode (as shown in the code fragment above) I always get a timeout in the next command:if (HAL_CAN_Transmit(&hcan, 10) != HAL_OK)
The function returns: HAL_CAN_STATE_TIMEOUT
All initialization seems to be ok (all functions return HAL_OK).
Analysis
What I tried was:- Using another STM32: no difference
- Using another transceiver: no difference - Played a bit with the SJW/BS1/BS2 time quantities: no difference - Making sure the time quantities were equal - Playing with different data values and filters: no difference - Checked the output of PB9 (CAN transmit): it seems not to change at all (so this is a problem): no difference - Removing the wire from GPIO PB9 (CAN Tx) to the TX of my CAN transceiver : no difference. - Checking the Transmit is cancelled (which is needed and was an old bug, but has already been fixed by the HAL library I'm using).Observations
- ESR is 111110000000000001010111, which means LEC[2:0] (see [Reference manual, page 682][1]), is 101 which is Bit dominant error
- BTR is 11101010000000001001111, which means bit 30 LKBM: Loop back Mode (debug) is 1, which is strange because in the setup I assigned CAN_MODE_NORMAL. - Directly after the command, the State is HAL_CAN_STATE_TIMEOUT, the Lock is HAL_UNLOCKED, the ErrorCode is 0.Questions
1. Why do I get a timeout? I'm having a hard time trying to find more to check what I already did. What bothers me is that the PB9 GPIO does not change, so I'm sure it's a software problem, but since there is no error code (it's 0) and initialization is OK, I'm getting out of clues.Related question:
2. Am I in loopback mode or not (according to the Setup I put CAN_MODE_NORMAL, but the BTR bit 30: LKBM shows otherwise.
[1]:
#can #stm32f103 #stm32cube2017-10-22 5:43 PM
Turvey.Clive.002
I found something stupid: my CAN receiver works on 5V and my STM32 is 3.3V, so I added a voltage supply that gives 5V and use that for the CAN transceivers (and connecting all grounds together). But still no difference. I ordered specifically 3.3V CAN transceivers and will try again when they arrive (can take some time).
2018-05-02 9:57 AM
stm32f103c8t6 + cubemxçš„can通信,我é�‡åˆ°è¿‡å’Œä½ æž�其类似的问题,已ç»�解决。我在æ¤è®°å½•æˆ‘çš„è§£å†³è¿‡ç¨‹ï¼Œå¸Œæœ›å¯¹ä½ æœ‰å¸®åŠ©ï¼š
第一个é�?™è¯¯ï¼šç�?¨äº†é»˜è®¤çš„CAN_TXå’ŒCAN_RX。开å�‘æ�¿ä¸Šå·²ç»�将这两个引脚分é…�给了USB接å�£ã€‚而ä¸�?USB上连ç�?µé˜»ç‰å…ƒä»¶éƒ½å·²ç»�有了,å¤�ç�?¨èµ·æ�¥ä¼šå¾ˆéº»çƒ¦ï¼Œæ‰€ä»¥åº�?该将CAN进行remap,转到PB8å’ŒPB9。(很显然,这一æ¥ä½ å·²ç»�å�šäº†ï¼‰
第二个é�?™è¯¯ï¼šæˆ‘ç�?¨çš„第一å�—å¼€å�‘æ�¿ï¼ŒPB8å’ŒPB9的两个引脚,ä¾�然没安排å�šäº†å…¶ä»–ç�?¨é€�?。这是我自己没ä»�?细看开å�‘æ�¿åŽŸç�†å›¾çš„å�Žæžœã€‚事已至æ¤ï¼Œä¸�å¾—ä¸�æ�¢ä¸€ä¸ªæ›´ç®€æ´�的开å�‘æ�¿äº†ã€‚
第三个é�?™è¯¯ï¼šcané…�置的时候,没有开å�¯SCE䏿–,以å�ŠRX0䏿–。当然,ä¸é€�?还出现了给CANæ�?¶å�‘器ç�?¨3.3Vä¾›ç�?µçš„低级é�?™è¯¯ã€‚
然�,我就进入了如楼主所�述的状�。
实际上这时候我é�‡åˆ°çš„æ˜¯ç¬¬0个é�?™è¯¯ï¼š
使ç�?¨cubeMX,我选择了freeos,开å�¯äº†can+master(PB8+PB9)。ç�?±äºŽæˆ‘需è¦�ç�?¨st-link进行调试,所以SYS分æ�?¯æˆ‘设置为“serial wireâ€�,并选择了TIM4作为定时器时钟æº�。然å�Žç�?±äºŽå…¶ä»–功能的需è¦�,我开å�¯äº†PB3 PB4 PB5 PB6四个GPIO模å¼�â€�?â€�?â€�?â€�?è¿™ç§�é…�置的å�Žæžœå°±æ˜¯SYS分æ�?¯ä¸Šå‡ºçŽ°äº†ä¸€ä¸ªé»„è‰²æ„Ÿå�¹å�·ã€‚
真æ£è§£å†³å…³é�?®é—®é¢˜çš„æ¥éª¤ï¼Œå°±æ˜¯å�–消掉PB3 PB4 PB5 PB6的使ç�?¨ï¼ŒæŠŠå®ƒä»¬æ�¢å¤�æˆ�默认的reset状æ€�,SYS上的黄色感å�¹å�·å°±æ¶ˆå¤±äº†ã€‚å†�å¾€å�Žå°±ä¸€åˆ‡æ£å¸¸äº†ã€‚
2018-05-02 6:37 PM
did you get this running ?
ABOM should be enabled.
2018-05-06 12:34 PM
To the above replies(write in Chinese), I made the following clarification: My project was not completely successful. It seems there is a bug in the HAL library .
Hardware configuration : stm32f103c8t6 processor, using cubeMX generated project, stm32F1 cube version number 1.6.1. Two TJA1050 work as CAN tranceiver.
The test proccedure is: Device A and Device B are interconnected. A initiates the first session and sends the numbers 0 to B. While B received the message, B sends 1 to A, and A sends 2 to B again... and so on.
The test result: A power on first, then ,B power on, and B can receive the message sent by A. B can send a message, debugtrace on B show success, but A can not receive the message
If B power on first and then A power on, B will not receive A message. Since the first message was initiated by A, there was no result in this round of testing.With the same hardware, a simple test program was written using the std library. The test target was exactly the same as above. The test was completely successful.
2018-05-10 5:45 PM
Make sure the two boards never transmit the same MsgID.
make sure ABOM is enabled
2018-05-11 8:00 AM
I don't think ABOM = ENABLE is necessary.
I changed the 'ping-pong procedure' ,it works like this:
A send '0' to B
if A received '1',A send '2' to B
or A will send another '0' after few seconds.
Once B received '0',B reply '1' to A.If B received '2',B reply '3' to A ,like 'Ping-Pong test'
Debug trace on B, I can see B received many '0' ,and B try to send '1' to A.HAL_CAN_Transmit_IT orHAL_CAN_Transmit returns OK, but A receive nothing.
I will try your suggestion.But it seems could hardly to be succeed.
======================================
test faild
code in Attach.
readme.txt will tell you how to build and test
________________ Attachments : Src.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxdq&d=%2Fa%2F0X0000000b0P%2FaWDD42Azorv0fh8l75LjtiEnKTKsTuQoTGhgmTEgkH4&asPdf=false2018-05-11 5:07 PM
do you have a scope ?
can you check that both units are transmitting first ?
2018-05-11 7:16 PM
I have no scope.
I just use debug trace ,set a break point on the send or receive function,and watching the message.
Trace on device B while A is running free or trace on device A while B is running free.
The same way ,using std library ,ping-pong test works.
2018-05-11 11:32 PM
I use a TDS2024, a 4ch color scope, excellent unit.
You need a scope for low level drivers.
2018-05-12 6:07 AM
ABOM should be enabled
Do you have another CanBus peripheral ?
I purchased a CanDo unit and transmitted every second to get the receiver code running first.
Then I worked on the Tx side.
My receiving code runs under interrupt control, but the transmit code doesn't.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.