2011-02-03 5:25 PM
I know that this forum is for the Discovery but I have a question regarding the STM3210C-Eval board, which is similar, and for which there is no forum.
I've been working with a small STM32 board, programming it with Atollic TrueStudio and the DeFUse Demonstration software. Slow work but making progress. I decided to speed things up by buying an STM3210C-Eval board and an ST-Link. The evaluation board powers up fine and runs the demo software. The ST-Link shows up as a USB drive on my computer with ST internet links on it. All good.I connect the JTAG ribbon cable from the ST-Link to the evaluation board, plug the ST-Link into the USB and then the power to the evaluation board. Using the STM32 ST-Link Utility I try to connect to the board but I get an ''STLink USB communication error'' every time. I have made sure that the setting is for JTAG (although I checked SWD as well for a laugh). Also disconnected the ST-Link from the computer and got another error instead so the ST-Link is definitely visible and working.
I switched to another computer in case there was a problem with USB drivers but still had the same problem.
Has anyone got any ideas as to what is going wrong here? A simple newbie problem? A dud ST-Link?
#stm32f107 #jtag #debugger #error #usb2011-02-03 7:38 PM
Stupid questions, but, you are using CN13 for JTAG, right? There is also a CN12 with is for trace tools. Both connectors have the same number of pins. Easy to get into the wrong connector.
Good luck, Jim2011-02-06 12:59 PM
There are no stupid questions, Jim. Thanks for the suggestion.
There is only one such connector in the ST-Link package, which I am going to have to assume is a CN13 for JTAG. Probably a safe assumption since it's the ST-Link's primary purpose.
Cheers
Huub
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.