2016-02-24 5:59 AM
Hi,
I am using SPI to send data between an STM32F411RE and a Raspberry Pi 2, using the HAL library on the STM and the Python frontend of spidev on the Pi. With this I can send or receive arbitrary amounts of data between the two. However, when I switch between transmitting and receiving, the two communicators get out of sync by one byte, and I have been trying to figure out why. The following code should send the same array of 20 numbers back and forth between the STM (slave) and the Pi (master): in main(): uint8_t buffer[20]; while (1) { HAL_SPI_Receive(&hspi1, buffer, 20, 1000000); HAL_SPI_Transmit(&hspi1, buffer, 20, 1000000); } void MX_SPI1_Init(void) { hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_SLAVE; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLED; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED; hspi1.Init.CRCPolynomial = 10; HAL_SPI_Init(&hspi1); } on the Pi: import time import spidev spi = spidev.SpiDev() spi.open(0,0) spi.max_speed_hz = 100000 spi.mode = 0b00 data = range(0,20) while True: print data spi.writebytes(data) data = spi.readbytes(20) time.sleep(0.5) When I run this, I always get [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 18, 19] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 18, 19] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 18, 18] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 17, 17] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 16, 16, 16] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 15, 15, 15, 15] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 14, 14, 14, 14, 14] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 13, 13, 13, 13, 13, 13] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 12, 12, 12, 12, 12, 12, 12] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 11, 11, 11, 11, 11, 11, 11, 11] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 10, 10, 10, 10, 10, 10, 10, 10, 10] [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 9, 9, 9, 9, 9, 9, 9, 9, 9, 9] [0, 1, 2, 3, 4, 5, 6, 7, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8] [0, 1, 2, 3, 4, 5, 6, 7, 7, 7, 7, 7, 7, 7, 7, 7, 7, 7, 7, 7] [0, 1, 2, 3, 4, 5, 6, 6, 6, 6, 6, 6, 6, 6, 6, 6, 6, 6, 6, 6] [0, 1, 2, 3, 4, 5, 5, 5, 5, 5, 5, 5, 5, 5, 5, 5, 5, 5, 5, 5] [0, 1, 2, 3, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4, 4] [0, 1, 2, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3, 3] [0, 1, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2, 2] [0, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1, 1] [0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0] [0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0] [0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0] [0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0] [0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0] though I would expect infinite repetitions of the first line. Unfortunately, I cannot be certain whether the issue is on the STM or the Pi. Have you seen this behavior before and/or can you explain it? #no-hablo-hal #spi2016-02-24 6:18 AM
Even with a simple echo it takes one byte time for the data to clock out completely and be received at the other end.
There could be some other issues deeper in the HAL (TXE/RXNE). I'd start be sending a fixed pattern back, and look at how the CS line can be used to synchronize the starting point.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.