2016-01-20 11:53 PM
Hi everyone ,
I develop FatFs file system on SST26VF016B 2MB SPI Flash.I have done raw read/writes. I can success Fully read/write all SPI flash addresses. My problem is i create file system and i create file but i'm not write any data on file.Because disk is full error. I am using this define in ffconf.h &sharpdefine _MIN_SS 512 &sharpdefine _MAX_SS 512 My diskio.c implementation like this, DRESULT disk_ioctl ( BYTE pdrv, /* Physical drive nmuber (0..) */ BYTE cmd, /* Control code */ void *buff /* Buffer to send/receive control data */ ) { DRESULT res; uint8_t status; status=SST_Status(); switch(cmd) { case CTRL_SYNC: if(status & 0x01) res=RES_ERROR; else res=RES_OK; break; case GET_SECTOR_COUNT: *(DWORD*)buff=4096; res = RES_OK; break; case GET_SECTOR_SIZE: *(WORD*)buff=512; res = RES_OK; break; case GET_BLOCK_SIZE: *(DWORD*)buff=1; res = RES_OK; break; }; return res; } and i use f_mkfs('''',0,4096); Whats the wrong?Why i get disk_full error? Thanks for help Best Regards #stm32 #fatfs #spi-flashWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.