2024-11-25 2:37 AM
Dear ST,
I use STM32F777 and try to receive SPI Data as a slave via SPI DMA. That works only pretty fine, when I don't activate the CRC Checksum calculation. I receive after the DMA threshold the expected data, but when I set:
Poly is 0x1021
Inti value is 0x0000
If I use the CRC HW Unit via SW, that works as well. But I still have to use the combination of DMA and CRC, because that part is on our application, very time critical. I still can not use the CPU instead.
2025-05-12 4:38 PM
The CRC is NOT going to be in the DR, the DR is 8-bit in your configuration.
If you're sending the data with the CRC, you send the data payload, and then once that is gone you read the TX CRC register, and send that.
The way you're describing it you sound like you want to receive four bytes and respond with the CRC.
In the receive sense, I'd expect you'd have to receive SIX bytes, and then the CRC will ZERO out
If you sent the 0xA5 0xA6 0x8C 0x00 0x07 0xFA pattern, the CRC correct check being the bit that checks RX CRC==0
I agree that the CRC16 for 4-byte MSB First should be 0x07,0xFA
ST should probably provide the validated test cases, I'm not invested to build a complete example
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.