2016-09-05 1:19 AM
As the title says, I'm wanting to set the Ethernet chip to enable DHCP and set its MAC address.
As I understand it - and I may well be wrong, so I'd be grateful for correction if I am - the chip manages the DHCP negotiations, all it needs is to be enabled to do this, and, of course, to have a MAC address set.I'm using Ada, so I don't have access to the C-library that does this - which is why I need to have more detail of how it works.I believe, again, correct me if I'm wrong, that I need to set a register, with the correct bit and correct address. I don't know which register I need to set.What is the correct register - or, even better, where is there documentation that gives the address of the register, and the register contents? #ethernet #dhcp #mac #stm32f72016-09-05 8:04 AM
Hi,
You can refer to the in section (38.8 Ethernet register descriptions) and (38.8.5 Ethernet register maps).RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.