STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX Audio Class

Posted on April 17, 2015 at 12:13Dear all, I'm trying to use STM32CubeMX software to have a starting point to realize a device like an USB Sound Card recognized by PC and able to play a music stream (as development board I'm using the STM32F4 Discov...

aressia by Associate II
  • 2295 Views
  • 4 replies
  • 0 kudos

How to Set USB CDC Line Coding?

Posted on August 02, 2016 at 05:11Using STM32CubeMX 4.16.0  I generated a project with the USB_DEVICE Communication Device Class option enabled. In the document at: http://www.st.com/content/ccc/resource/technical/document/user_manual/b8/5a/28/c2/c...

spflanze by Associate II
  • 2058 Views
  • 1 replies
  • 0 kudos

How use one USB port to update firmware for two MCUs

Posted on July 28, 2016 at 08:12Hi,   Two questions:1. There are two MCUs on my board, they are STM32F072RB and STM32F042C6. However, my master computer has only one USB port which is integrated in a box with my board. If use two ports to update 2 M...

zhipan by Associate II
  • 2563 Views
  • 4 replies
  • 0 kudos

STM32 USB OTG MSC

Posted on April 19, 2016 at 18:00 Hi, I'm using an STm32F107 and I trie to configure the USB interface as host to access to an key. This is the initialization code : MX_USB_HOST_Init(); MX_FATFS_Init(); with : ...

b2399 by Associate II
  • 2124 Views
  • 4 replies
  • 0 kudos

wfi instruction kills RTOS

Posted on July 29, 2016 at 04:22I have the 32F746G DISCOVERY. I am using IAR tools.I�m using that PCB to adapt my STM32F4xxx RTOS to the Cortex-M7 product line. I had a bit of trouble putting my ROM image at 0x0800000 and my RAM starting at 0x200000...

picguy2 by Associate II
  • 1118 Views
  • 1 replies
  • 0 kudos

Bootloader and STM32F091

Posted on July 27, 2016 at 17:24 Hi everybody, I try to make a bootloader with my STM32f091 to copy a new firmware to my boards using the Power Line Current. First, I bought the evaluation kit (STEVAL-IHP005V1), it works very without a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.