2015-03-27 2:03 PM
I have an STM32F427 using the 1.4 version of the STMCube software with the HAL drivers.
I am using the stock 1.4 and calling HAL_SD_ReadBlocks_DMA to transfer 1 block from the SD card. Periodically, it hangs in the following function waiting for the SD transfer to complete:static void SD_DMA_RxCplt(DMA_HandleTypeDef *hdma){ SD_HandleTypeDef *hsd = (SD_HandleTypeDef*)((DMA_HandleTypeDef*)hdma)->Parent; /* DMA transfer is complete */ hsd->DmaTransferCplt = 1; /* Wait until SD transfer is complete */ while(hsd->SdTransferCplt == 0) <----- hangs forever { }...It happens one time out of maybe 1000 times when transferring one block. When transferring more than one block in the ReadBlocks_DMA... call, it hangs one time out of 50.It looks like the DMA and SD command are setup correctly, but the SD complete status is never set in the HAL_SD_IRQHandler. When it hangs like this, it appears that the SD IRQ Handler is never called with the SDIO_IT_DATAEND flag.I am using DMA for ethernet as well, but that is on a different DMA channel.I have the SD and DMA interrupt priorities set the same as the v1.4 code.Any thoughts?Thanks...Keith #sdio #stm32 #fatfs2016-06-07 4:42 AM
Hi rhodes.keith,
I suggest that you take a look to this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32Cube%20%2B%20F4-Discovery%20%2B%20FatFS&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=107]thread -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.