STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F05 USB No more interrupts

Posted on May 11, 2016 at 11:36I found a very interesting situation, I can't explain (so no solution). We have a project and the USB connection is lost. Disconnecting and reconnecting the cable will not solve the situation and after the reconnection...

0690X00000604ePQAQ.png 0690X00000604uWQAQ.png
alin1 by Associate
  • 1594 Views
  • 1 replies
  • 0 kudos

USB Device Library. Beginner question

Posted on May 12, 2016 at 12:44Hello friends!I'm working on implementing USBTMC class USB Device Library. The question was how to implement the transfer of bulk-out. According USBTMC specification: ''... If the last data payloadis wMaxPacketSize, th...

Tim 15 reset timer 1.

Posted on May 10, 2016 at 18:52Hi everyone.I'M using a STM32F302CB. I'm using many timers in the application. I had a problem that I find a solution with 2 timers, but I don't understand the reason why.Timer configuration: The timer 1 is using to ...

jf2 by Associate II
  • 2280 Views
  • 4 replies
  • 0 kudos

Multichannel ADC

Posted on May 06, 2015 at 19:17 Hi, I'm developing application on STM32F0 where I use two gas sensors (CO and CO2), so I need two channels on ADC. In my main.c I only call two functions and on beginig of each function I change channel like so: ...

muliku by Associate II
  • 5288 Views
  • 10 replies
  • 0 kudos

STM32 Touch Sensing Library Example Touchkey

Posted on May 12, 2016 at 01:02I am looking for any example of TouchKey application on any STM32 using Touch Sensing Library. Preferably using code generated by STM32CubeMX. Anyone? Any clue? Thank you. #stm32-cube-touch-sensing-library

ekawahyu2 by Associate II
  • 1195 Views
  • 1 replies
  • 0 kudos

Virtual Comport Driver

Posted on April 08, 2016 at 07:21Hi. we are using the VCP1.4.0 Driver to use STM32F042 USB SERIAL. But , in the Windows 10, driver happen some strange behavior. For example, when we disconnected the usb port, Windows CPU load goes up suddenly. So we...

yymo1019 by Associate II
  • 1880 Views
  • 3 replies
  • 0 kudos

STM32L476 had too much coffee

Posted on May 06, 2016 at 22:49I have been trying to implement the Tickless Idle feature in FreeRTOS (which comes pre-implemented for STM32 processors).In my main code I have turned off all IP except the pushbutton (EXTI0), which I want to use to wa...

mattreed9 by Associate III
  • 1184 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.