2021-02-22 12:08 AM
Hi
I have setup SDMMC1 over DMA2 channel 14 (Tx) and having issue in writing more frequent data. I have interrupt on system tick (pend sv) 1ms. When I write every 10ms 128 Bytes, it gives me ring buffer overflow error. That means it stuck somewhere on f_write and not returning from there.
I have found that it gives timeout on
HAL_DMA_PollForTransfer(&SDMA__stDMA_Copy_handle, HAL_DMA_FULL_TRANSFER, 1000) function after starting DMA transfer.
Is it related to FATFS or DMA ?
Is there any workaround to write more frequent large data with current configuration.
I have set DMA interrupt priority as 6 and SDMMC1 as 5.
Any help would be appreciated.
2021-03-30 12:21 AM
Hello, sometimes sdcard needs a lot of time for writing. Try to increase the time beetween writing (like 500ms) for testing. Also, you can try increasing your buffer size.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.