2015-06-05 10:54 AM
I was able to compile and run the code provided by Tilen from
http://stm32f4-discovery.com/2014/07/library-21-read-sd-card-fatfs-stm32f4xx-devices/
, So I can mount , write and read data from file. But when I measured the throughput the measurement was very disappointing for read operation I got only 500KB/s which is lame for an SDIO operation, I calculated the throughput but toggling a GPIO before and after read/write operation, for example GPIO_SetBits(GPIOD,GPIO_Pin_4); f_write(&fil,data_buffer,10240,&written) GPIO_ResetBits(GPIOD, GPIO_Pin_4); Is there something that I need to do , in-order to get a better throughput about 5-7MB/s #stm32 #dma #!stm32f4-disco #fatfs #sdio #sdWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.