2026-01-14 8:03 AM - edited 2026-01-14 8:08 AM
I have a bunch of following warnings:
c:/programs/ARMtools/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.stm32/STM32F1xxxx/STM32F1xx_HAL_Driver/Inc/stm32f1xx_ll_gpio.h: In function 'void LL_GPIO_SetPinMode(GPIO_TypeDef*, uint32_t, uint32_t)':
c:/programs/ARMtools/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.stm32/STM32F1xxxx/STM32F1xx_HAL_Driver/Inc/stm32f1xx_ll_gpio.h:343:22: warning: ISO C++17 does not allow 'register' storage class specifier [-Wregister]
343 | register uint32_t *pReg = (uint32_t *)((uint32_t)((uint32_t)(&GPIOx->CRL) + (Pin >> 24)));
|in several LL headers.
Can this please be fixed in some suitable way? One way to do that might be to replace the 'register' specifier by a macro, which would be defined based on the __cplusplus standard preprocessor macro and its value. A simple version would be to add
#if __cplusplus >= 201703L
#define register
#endifto each header where this occurs, but I am not a C++/build-environment specialist so don't know whether this may have some unwanted effect I am not aware off.
Thanks,
JW
2026-01-14 8:18 AM - edited 2026-01-14 8:27 AM
Same Issue recently:
HAL functions using archaic terms - why?
(the "archaic term" is the register specifier)
PS:
and from 2018:
Is the "register" storage class specifier necessary in STM32 LL interfaces?
TL;DR: No.
2026-01-15 12:56 AM - edited 2026-01-15 1:01 AM
Hello @waclawek.jan ,
Please refer to the package available on GitHub. it has been updated and this item has been removed from the header file: stm32f1xx_ll_gpio.h
Please download the latest version of the package from the GitHub page.
thank you!
Hamdi
2026-01-15 1:10 AM
Is it just the F1 that's been updated?
The other linked threads refer to U0 and L4
Presumably (all?) others are similarly affected?
2026-01-15 1:13 AM
hello @Andrew Neil
Yes, all of them have been updated, not just the F1.
The same change has been applied to the other affected series.
thank you!
2026-01-15 5:21 AM
Hi @T_Hamdi ,
thanks, that would solve it for this particular header file.
But what about other headers, e.g. https://github.com/STMicroelectronics/stm32f1xx-hal-driver/blob/a433ed968f1812eff2de76288af48aab2e369e9f/Inc/stm32f1xx_ll_rtc.h#L553 ?
JW
2026-01-15 8:24 AM
Hello @waclawek.jan
Thank you for bringing this issue to our attention.
I reported this internally. Internal ticket number: 225259 (This is an internal tracking number and is not accessible or usable by customers).
Best regards,
Hamdi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.