2019-04-24 3:11 AM
Hi,
I am using firmware package of USBPD_F0_V2.1.0 for utilising Power delivery by TCPM/TCPC configuration, using the example application. During initialisation- debugging of USBPD_DPM , I get an error code of USBPD_StatusTypeDef of 0x22 which is USPD_MALLOCERROR. This error comes from the function of USBPD_TCPM_HWInit which initialises the TCPC drivers in usbpd_dpm_core file. I would like to know what is the source of this error. I am using heap_4.c and the heap size is more than enough for memory allocation. What can be the reason of malloc error in USBPD_TCPM_HWInit function? I am using a heap size of 4200 bytes with dynamic allocation set to 1.
2019-04-26 7:34 AM
Thanks a lot by the way with the help so far!
2019-04-26 8:00 AM
Found a information here... Do you syscall.c in your environment? if yes, do you have function '_sbrk' inside?
2019-04-29 2:31 AM
Hey Yohann,
Thanks again. Yes I have the syscalls.c file in my environment within the project. And it has the _sbrk function where the heap management is done. I have checked the project settings and I have the -specs=nosys.specs settings and i couldn't delete this from the linker settings. Do you know how i can edit this in true studio? Besides when i comment out the _sbrk function in sys calls.c, the malloc works fine, so does the USBPD_TCPM_HWInit() function. Is this a good solution? or i may face problems regarding the stack collision management?
2019-05-02 7:58 AM
Hello mynja
We checked the TrueStudio User Manual and in page51, there is a recommendation to generate Syscall when RTOS is used.
I suggest to use the following code in your syscall.c:
#define FreeRTOS
#define MAX_STACK_SIZE 0x500
extern int __io_putchar(int ch) __attribute__((weak));
extern int __io_getchar(void) __attribute__((weak));
#ifndef FreeRTOS
register char * stack_ptr asm("sp");
#endif
caddr_t _sbrk(int incr)
{
extern char end asm("end");
static char *heap_end;
char *prev_heap_end,*min_stack_ptr;
if (heap_end == 0)
heap_end = &end;
prev_heap_end = heap_end;
#ifdef FreeRTOS
/* Use the NVIC offset register to locate the main stack pointer. */
min_stack_ptr = (char*)(*(unsigned int *)*(unsigned int *)0xE000ED08);
/* Locate the STACK bottom address */
min_stack_ptr -= MAX_STACK_SIZE;
if (heap_end + incr > min_stack_ptr)
#else
if (heap_end + incr > stack_ptr)
#endif
{
// write(1, "Heap and stack collision\n", 25);
// abort();
errno = ENOMEM;
return (caddr_t) -1;
}
heap_end += incr;
return (caddr_t) prev_heap_end;
}Regards,
Yohann
2019-08-23 5:13 AM
Hey Yohann,
WE are still working on the same project with TCPM/TCPC architecture. Indeed we are trying to establish firmware with PortNumbers=8. WE are getting USBPD_ERROR when the number of ports is 3. We realised that there is internal USBPD_MAXPORT_COUNT within the code and we could not find this definition in the library. What is this number and is there a way to change it? It is important for us since we need to use 8 Ports configuration.
Thanks in advance.
Best Regards,
Faik
2019-08-26 6:02 AM
Hi Faik,
You are right, we have limited max of ports number to 2 (for memory footprint mainly). We will remove this dependancy in a future library delivery.
For your information, even I2C allows to use a big list of slaves, you could have a latency issue to answer in the good timeframe to a PD message (refer to study done in USB DevDays presentation done in 2015, https://manualzz.com/doc/12523600/usb-type-c%C2%99-port-controller--tcpc--for-usb).
Regards,
Yohann
2019-08-27 5:25 AM
Hey Yohann,
Thanks for your quick response! I would like to ask if there is a possibility for you to edit the library to be used for max ports number of 8 and we can do the testing and debugging in exchange for you? This may speed up the process for both sides i think. Otherwise, do you know when there will be the updated library delivery?
I will also have a look into latency issues may arise for i2c.
Best Regards,
Faik.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.