2026-01-28 4:47 PM
Hello everyone, I'm having some trouble implementing I3C communication and would like to ask for some help.
I am using the NUCLEO-H503RB board as my main controller. For the target devices, I have the NUCLEO-IKS01A3 expansion board and the TSC1641 (Click Board) connected. I'm currently facing some issues with the I3C communication setup between these components.
I have successfully managed to read the WHO_AM_I ID from the LSM6DSO (on the NUCLEO-IKS01A3). However, when I attempt to read the ID from the TSC1641, the SCL line continues to output a clock signal (or stays toggling) without a proper response. I am seeking assistance in analyzing the root cause of this issue.
Solved! Go to Solution.
2026-02-20 7:01 AM
Hello @roro ,
@roro wrote:
I am using the NUCLEO-H503RB board as my main controller. For the target devices, I have the NUCLEO-IKS01A3 expansion board and the TSC1641 (Click Board) connected.
How did you connect NUCLEO-IKS01A3 expansion board and the TSC1641 to NUCLEO-H503RB board? did you manage to check some hardware conflicts by referring to the different schematics?
2026-02-20 7:01 AM
Hello @roro ,
@roro wrote:
I am using the NUCLEO-H503RB board as my main controller. For the target devices, I have the NUCLEO-IKS01A3 expansion board and the TSC1641 (Click Board) connected.
How did you connect NUCLEO-IKS01A3 expansion board and the TSC1641 to NUCLEO-H503RB board? did you manage to check some hardware conflicts by referring to the different schematics?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.