2024-04-16 8:33 AM - edited 2024-04-16 8:50 AM
[EDIT: S'OK, I need to think about this more, but I can't find a way to delete a message so am just marking this as one to ignore]
I am just moving from STM32F4 to STM32U5. ThreadX seems to be the thing for STM32U5 (if one doesn't want to use Zephyr) but I need to be able to use FreeRTOS also, so I have moved all of my code to CMSIS (V2). However, I am not able to find cmsis_os.h/cmsis_os2.h for ThreadX. For instance, in the STM32F4 case the CMSIS API for FreeRTOS can be found under the Middlewares/Third_Party/FreeRTOS/Source directory.
The STM32CubeU5 only contains "template" cmsis_os.h/cmsis_os2.h files but I don't want a template of my RTOS interface, I want the actual RTOS interface that ThreadX will abide by. The cmsis_rtos_threadx directory of STM32CubeU5 only contains the .c file, no headers. The ThreadX repo doesn't contain a CMSIS adaptation at all.
Where do I find the CMSIS adaptation API that ThreadX will abide by?
Solved! Go to Solution.
2024-04-16 9:09 AM - edited 2024-04-16 9:11 AM
Have you found the FreeRTOS adaptation layer for ThreadX?
and here is the CMSIS RTOS .c
2024-04-16 9:09 AM - edited 2024-04-16 9:11 AM
Have you found the FreeRTOS adaptation layer for ThreadX?
and here is the CMSIS RTOS .c
2024-04-16 9:09 AM
Hello @Rob Meades ,
Maybe think about and we will be happy to help. if you have any updates maybe comment on this thread.
BR
2024-04-16 9:12 AM
@Pavel A: ah, _that's_ where it is, I was going to steal the one from STM32F4 and hope for the best; that's much better.
@STea: thanks, I will.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.