2022-11-07 10:25 PM
I want to store some data into flash (read/write)..i have no idea wheter it can be done with Nucleo L433RC-P DK. if possible plz share the example code
i tried with an example code (github - controllerstech F1, F4, H7 series) . but no use of it
2022-11-08 3:41 AM
Hello @Nagendra A Karmarkar and welcome to the Community :)
You can use the available "Flash" example within STM32CubeL4 package:
STM32Cube_FW_L4_V1.17.2\Projects\NUCLEO-L432KC\Examples\FLASH\FLASH_WriteProtection
Hope this helps you!
When your question is answred, please close this thread by choosing Select as Best. This will help other users find that answer faster.
Imen
2022-11-08 11:12 AM
> i have no idea wheter it can be done
Then try reading the reference manual!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.