STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Where can I find the "generate_OoB_hexfiles.bat" file described on the STM32F7508-DK demonstration library?

I cannot find the script generate_OoB_hexfiles.bat refereed at the STM32F7508-DK demonstration library. On the other hand, This script is only used for concatenate hex images to an only one hex image, and I want to know more about this process. Pleas...

vicfer89 by Associate II
  • 2501 Views
  • 4 replies
  • 0 kudos

Resolved! Why is DMA peripheral to memory option not available when configuring my project in CubeIDE?

I'm working through ST Application Note AN5027 (link) to interface PDM microphones via SAI (specifically, the example given on p41 onwards). I selected a Nucleo L4A6ZG for this, due to it having SAI, but I'm having some trouble following the DMA con...

[BUG] in STM32CubeF7 EEPROM_Emulation Project: Function EE_VerifyPageFullyErased() can't verify if PAGE1 is erased.

Hey All,I'm using the STM32CubeF7 v1.15.0 Lib.If I look in any EEPROM_Emulation Project in the file eeprom.c, there is all the time the same issue with the function EE_VerifyPageFullyErased() starting at line 328:/** * @brief Verify if specified p...

jwoerle by Associate III
  • 3907 Views
  • 7 replies
  • 1 kudos

Resolved! Firmware download for 32F769I-DISCO

I have an unused 32F769I-DISCO board which I think needs firmware programming - it sits with a flashing red LED when power is applied. The only support I can find is for the 32F769NI-DISCO board which is slightly different and the "Getting started" v...

AWood.4 by Associate
  • 1886 Views
  • 2 replies
  • 0 kudos

Accessing files via FTP on STM32U5

Hi,We're trying to access files from STM32U5 over FTP - at the moment we're using the b-u585i-iot02a discovery kit alongside AzureRtos/Middleware. Just wondering if there already exists an example code that could assist us in getting a head start. Se...

UKhan.2 by Associate II
  • 2200 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.