2016-01-03 7:01 PM
I am trying to plug a Nucleo F303RE into an Android 6.0 phone and connect to the CDC port via an Android application.
Bad things happen when I do this. Apparently Android 6.0 detects the ST/LINK mass storage device and automounts it, then writes something to the mass storage device which causes the ST/LINK to erase the Nucleo's firmware. I have to reprogram the Nucleo to use it again.Is there any way to prevent the ST/LINK from enumerating the mass storage device or have the CDC operate without the ability to flash the Nucleo?I have tried removing the jumpers from CN2. When I do this, the Nucleo in inoperable until the ST/LINK MCU is reset and then the CDC is not enumerated. #android-usb-otg-st/link-nucleoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.