STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error in stm32f3xx_hal.h

Posted on December 10, 2015 at 15:15Into HAL driver V1.2.0/November-2015 not defined standard type declarations. Insert include file stdint.h in stm32f3xx_hal.h to solve this problem.In System Workbench, compiler and maker not cancel building proces...

mistake in stm32f3xx_hal_pcd.c

Posted on December 08, 2015 at 10:56Hi, STM32Cube_FW_F3_V1.3.0\Drivers\STM32F3xx_HAL_Driver\Src\stm32f3xx_hal_pcd.c In the function below: static HAL_StatusTypeDef PCD_EP_ISR_Handler(PCD_HandleTypeDef *hpcd)     ... line 455:         /*multi-packet ...

thln47 by Associate III
  • 1032 Views
  • 1 replies
  • 0 kudos

HAL_Delay() not working.. help (newbie)

Posted on December 04, 2015 at 01:51Hi, I tried using HAL_Delay(); I thought I can just use HAL_Delay(500); but it's not working.the code is below. (from STM32cubeF4)__weak void HAL_Delay(__IO uint32_t Delay){  uint32_t tickstart = 0;  tickstart = H...

ckim by Associate II
  • 4032 Views
  • 3 replies
  • 0 kudos

HAL DMA Complete callback execution context?

Posted on December 03, 2015 at 15:48Maybe I'm blind but I couldn't find this info anywhere.When I get a HAL ''DMA Complete'' callback, is that code operating inside an ISR context or as normal user code?  I inherited some firmware code and it's doin...

STM32F7 - Discovery: DCMI Code Examples?

Posted on December 03, 2015 at 15:27I got the http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/LN1848/PF261641?icmp=pf261641_pron_pr-massmarket_jun2015&sc=stm32f7discovery-pr and the http://www.st.com/web/catalog/tools/FM146/CL1984/SC720/SS...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.