2024-04-12 7:23 AM
Hello,
I have encountered a peculiar problem and I am running out of ideas on what to do next.
I'm working on a project with an stm32H563 mcu and lan8742 phy, using threadX and netXduo.
When the code is first downloaded it runs fine, but after a power cycle it doesn't. Connecting a debugger shows that everything is running as expected except there are no ip_events generated. The condition
if (ip_events & NX_IP_RECEIVE_EVENT)in "nx_ip_thread_entry.c" stops triggering (ip_events never changes.)
The thing is, a few weeks ago everything was working fine, the application started up and ran as expected, it responded to pings and processed incoming UDP - it is still running on two of the boards I prepared back then (and I dare not touch those at the moment).
Now that I do the same thing with any of the other boards, all of which were working previously, the application boots and runs after programming, but if I cut the power and restart, it doesn't. It's the same code checked out from the same repo, compiled on the same computer. I've also tried other computers, both Windows and Mac OS, so it's probably not that. The only thing I know has changed are updates to CubeMX and CubeIDE, but I haven't seen any reports on recent breaking changes.
Any help or suggestions on where to dig would be greatly appreciated.
Cheers,
// Ola
2024-04-12 8:56 AM
Hello @olaan ,
can give us more information about the version of cubeMX/IDE that were working and the newer versions you are working with also I recommend checking the changes that need to be made in the linker files to properly allocate the memories. Check also the pin assignment for Ethernet and if it is according to the board schematics. it will be helpful if you can share about your code and how did you implement the configurations of the Ethernet and ThreadX AND NETX.
BR
2024-04-14 11:52 PM
Hello @STea and thanks for the reply!
2024-04-15 3:36 AM
So, a quick update.
I installed CubeIDE 1.14 (with CubeMX 6.10) ported the project and now it works as expected. Presumably there is some change introduced in 1.15 / 6.10 that breaks my project, though I'm not sure what it could be.
Cheers,
// Ola
2024-04-17 11:21 AM
My experience was similar...
-rob
2024-04-17 10:35 PM
Spot on. This is my problem exactly. I was pretty sure it was reproducible since I got it consistently on windows and Mac, but you've confirmed it.
Cheers,
// Ola
2024-04-18 8:54 AM
Hello @olaan ,
I confirm the issue, I reported the issue internally.
Internal ticket number: 179408. (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
2024-04-30 8:33 AM
Thank you!
Any ETA on when it will be fixed? I'd rather not update without knowing if my application will work.
Cheers,
// Ola
2024-05-13 8:59 AM
Hello @olaan ,
after further investigation we are unfortunately unable to reproduce your behavior.
if you can share the project to further examen what's happening it would be great.
Juste as a hint, when you opened your project with CubeIDE 1.15 did you perform an STLINK update to your board and if you did, did you change the clock speed because in this update we use clock speed 8.33Mhz and not the older 8Mhz value.
BR
2024-05-21 11:38 PM
Hello,
I did all the updates I could find at the time, so the ST-Link should also have been updated.
I have a project which demonstrates the problem. However, when we talked last time, it did not seem like the forum allowed me to upload it. Is there another way I could share it with you?
It is a bit strange that it could not be reproduced on your side. We could consistently recreate the issue by simply creating new projects and including the NetXDuo driver. Are there more recent versions available where it may have been fixed as part of some other issue? I hesitate to update without a reasonable chance it has been fixed.
Cheers,
// Ola
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.