2025-06-30 4:09 AM
hi
i am working with HTTPS client code on stm32u585 microcontroller, using netx tcp/ip stack for the implementation. my requirement is to create a HTTPS post request with a json payload( nearly 8000 bytes). is there any reference or example available on HTTPS post request using netx. all i can see is the get request in the official GitHub.
if any example or reference regarding this issue will be much helpful for implementation.
with regards
sabarinath
2025-07-01 4:49 AM - edited 2025-07-01 4:55 AM
HTTP messages are decoded in _nx_web_http_server_receive_data.c
Here GET and POST messages are selected
in case of POST, VOID _nx_web_http_server_put_process(NX_WEB_HTTP_SERVER *server_ptr, NX_PACKET *packet_ptr) is called
inside _nx_web_http_server_put_process() nx_web_http_server_request_notify() is called
You have to provide nx_web_http_server_request_notify() and assignto your HTTP server in nx_web_http_server_create()
/* Call the user supplied function to notify the user of the put request. */
status = (server_ptr -> nx_web_http_server_request_notify)(server_ptr, NX_WEB_HTTP_SERVER_PUT_REQUEST, server_ptr -> nx_web_http_server_request_resource, packet_ptr);
2025-07-01 5:15 AM
@mbarg.1 wrote:HTTP messages are decoded in _nx_web_http_server_receive_data.c
That's the server side; I think @sabari1 is asking for the client side - ie how to make the request ?
2025-07-01 6:41 AM
OOPS ..
@Andrew Neil is right.
As far as I know, no examples for this case.
I guess @sabari1 has to use TCP socket to send a packet with HTTP/HTTPS PUT request writing ad hoc code.
Later will have to manage server reply ...
2025-07-01 6:52 AM
@sabari1 It seems that NetX Duo has an HTTP Client:
Chapter 1 - Introduction to HTTP and HTTPS
This chapter introduces the NetX Duo HTTP/HTTPS for Web module:
Previously, in this forum:
Solved: ThreadX NetXDuo https client post request problem
Both via: https://www.google.com/search?q=netx+HTTPS+client
(other internet search engines are available)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.