2025-07-07 1:10 AM
Hella All,
While working with the STM32H533RE microcontroller and using VS Code with PlatformIO for debugging, I noticed that the SCB (System Control Block) peripheral definitions appear to be missing from the SVD file.
The SCB is a critical ARM Cortex-M33 core peripheral that should include registers such as:
The missing SCB definitions limit our ability to:
I would greatly appreciate your assistance in resolving this issue.
Best Regards,
ManiK
Solved! Go to Solution.
2025-07-07 3:21 AM
Hello @mani9989
We no longer support MCU core registers in our SVD files as they can be part of the IDE in use (IAR,Keil,CubeIDE, etc...).
It did create confusion in the past weather the user is using the MCU register's view integrated in the IDE or from SVD file, so we are now sticking to supporting only IPs related to STM32 products in our SVD files.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-07 3:21 AM
Hello @mani9989
We no longer support MCU core registers in our SVD files as they can be part of the IDE in use (IAR,Keil,CubeIDE, etc...).
It did create confusion in the past weather the user is using the MCU register's view integrated in the IDE or from SVD file, so we are now sticking to supporting only IPs related to STM32 products in our SVD files.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-13 11:16 PM
Hello @STTwo-32,
Thank you for the clarification.
Since SCB and other core registers are not included in the SVD file for STM32H5, could you please advise on the best way to access or monitor SCB registers (e.g., VTOR, AIRCR, ICSR) during debugging in VS Code with PlatformIO?
Specifically, I'm looking for guidance on:
How to inspect SCB register values during a debug session (e.g., trap cause, exception entry).
Recommended approach to capture trap/exception information like:
HardFault status (HFSR)
Configurable Fault Status (CFSR)
Bus Fault (BFAR)
MemManage Fault (MMFAR)
Any suggestions for manual mapping or watch expressions in the debugger that would allow me to monitor these registers, since they’re not shown in the peripheral view.
Any tips or best practices for bare-metal Cortex-M33 debugging without full SVD support would be greatly appreciated.
Best regards,
Manikanta
2025-07-14 12:39 AM
Hello @mani9989
This is a new question. So, you may create a new post for it (after selecting a best answer for this post) so your question have more visibility and more people may help you (ST experts and other community members).
Best Reagrds.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-14 1:07 AM
I raised this as a new topic thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.