2025-04-17 4:02 AM - edited 2025-04-17 4:08 AM
Hi, I'm running the following example project:
STM32Cube_FW_F7_V1.17.0\Projects\STM32F769I-Discovery\Applications\mbedTLS\SSL_Client
on the development board STM32F769I-Discovery.
Seems like the application uses the .h file
STM32Cube_FW_F7_V1.17.0\Middlewares\Third_Party\mbedTLS\include\mbedtls\config.h
to configure the embedTLS module.
The project also includes this .h file for configuration of mbedTLS:
STM32Cube_FW_F7_V1.17.0\Projects\STM32F769I-Discovery\Applications\mbedTLS\SSL_Client\Inc\mbedtls_config.h
But it doesn't seem like it's used, why is that?
BR
Jonas
Solved! Go to Solution.
2025-04-18 1:31 AM
In every mbedtls include file there is a check on MBEDTLS_CONFIG_FILE C define:
#if !defined(MBEDTLS_CONFIG_FILE)
#include "config.h"
#else
#include MBEDTLS_CONFIG_FILE
#endif
If it is defined, the file indicated in it is included instead of mbedtls\config.h
It is defined in the SSL_Client example project files : MBEDTLS_CONFIG_FILE=<mbedtls_config.h>
2025-04-18 1:31 AM
In every mbedtls include file there is a check on MBEDTLS_CONFIG_FILE C define:
#if !defined(MBEDTLS_CONFIG_FILE)
#include "config.h"
#else
#include MBEDTLS_CONFIG_FILE
#endif
If it is defined, the file indicated in it is included instead of mbedtls\config.h
It is defined in the SSL_Client example project files : MBEDTLS_CONFIG_FILE=<mbedtls_config.h>
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.