2017-08-11 11:55 PM
Hi
2 questions here:
1. Why do I need the osDelay(1) before netbuff_delete()? Without it I get a statistical bug/crash.
2. why do I need lines x1-x3. Without it no second connection is possible.
/*----------------------------------------------------------------------
-------------*/static void udpecho_thread(void *arg){ err_t err, recv_err;LWIP_UNUSED_ARG(arg);
uint8_t send_buffer[32]={0xff}; uint16_t len = 0; conn = netconn_new(NETCONN_UDP); if (conn!= NULL) { err = netconn_bind(conn, IP_ADDR_ANY, ARTNET_PORT);if (err == ERR_OK)
{ while (1) {recv_err = netconn_recv(conn, &buf);
if (recv_err == ERR_OK)
{ addr = netbuf_fromaddr(buf); port = netbuf_fromport(buf); len = netbuf_len(buf); if (len < 700) netbuf_copy(buf, &MyData, len); if (len > 32) netbuf_ref ( buf,send_buffer , 32); netconn_connect(conn, addr, port); netconn_send(conn,buf); // why do i need this delay?????????? osDelay(1); netbuf_delete(buf);//if I uncomment this 3 lines , every thing works fine
//X1 netconn_delete(conn); //X2 conn = netconn_new(NETCONN_UDP); //X3 err = netconn_bind(conn, IP_ADDR_ANY, ARTNET_PORT); } else { netconn_delete(conn); } } } }}#lwip #stm32 #netconn #free-rtosWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.