STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Firmware upgrade using SPI - STM32F7

Posted on June 26, 2017 at 17:25Hi everyone,I am trying to understand how the firmware upgrading works in the STM32F7 using a STM32F769I Discovery board. I would need to use the UART or SPI peripheral to upgrade.Does anyone know where to find exampl...

How to wake up the Uc through a USB plug interrupt?

Posted on June 30, 2017 at 08:54Hi,I am using the SMT32L476RG and my issue is relative to wake up the Uc from sleep mode through a USB plug interrupt.I am currently used the USB_Device_Library from ST (v1.0_Cube)Once I called MX_USB_DEVICE_DeInit();...

Omnia . by Associate II
  • 1064 Views
  • 0 replies
  • 0 kudos

Damaged? 2.5V at PA4 in Reset state (STM32F446VET)

Posted on June 29, 2017 at 11:58Hi,Im trying to optimize LowPower current consumption of a custom board my hardware guys have made arround a 100pin LQFP STM32F446VET. Currently I fight to find the source of a faulty voltage at GPIO PA4 (Pin 29 with ...

Miro Mico by Associate II
  • 3110 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F407IGT6 standard peripheral library PDF

Posted on June 27, 2017 at 05:41Hi,I am new to STM32 and want to learn STM32F4 but I could not find the standard peripheral library manual online.  I would like to see some explanations of the library functions and some examples.  Any help?  Thanks ...

j Q33 by Associate II
  • 3408 Views
  • 5 replies
  • 0 kudos

USB HID lost packets

Posted on June 28, 2017 at 22:47My STM32F427 project implements HID (FS device endpoint 1) USB communication and is developed with ST USB library v.2.2.0.It works fine, but during some periods (when continuous IN and OUT streams take place), some pa...

Getting Started With Ethernet.

Posted on June 20, 2017 at 13:48Hello everyone,I have recently switch from 8 bit to 32 bit ARM based MCUs. Currently i'm working on a project in which i want to create a LAN of some communicating devices and for this i have purchased STM32F4I-DISC1 ...

Resolved! UM1722 On semaphores example

Posted on June 24, 2017 at 19:07I am using cubemx v4.21.0. and the freertos version is 8.2.3. & the cmsis-rtos version is 1.02.I am using the examples of STM32F413ZH-Nucleo in stm32cube F4 v1.16.0 , when I download the program. It works wrong!I foun...

STM32F429 and DP83848 (LwIP)

Posted on June 23, 2017 at 21:00Hi friends.I have a problem. I implement LwIP and FreeRTOS to my STM32F429-Discovery kit, but program don�t work. And I would ask to you. Can anyone generate a bin file, with some test program? For example: Ping, some...

Resolved! LwIP UDP Define has no reference

Posted on June 22, 2017 at 17:28Hello fellow Ethernet explorersI am currently trying to make a UDP connection between a stm32f4 discovery board and a pc.I have already made an example work and I am now trying to replicate the result but with a progr...

andy b by Senior
  • 2084 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.